Data acquisition
Data management
Process monitoring & visualization
Data acquisition
Data management
Process monitoring & visualization
Field of Application
SupplyCare Enterprise SCE30B is a web-based operating program for the indication and monitoring of levels of e.g. tanks and silos spread all over the world.
SupplyCare Hosting is a software application hosted in the Endress+Hauser cloud for the indication and monitoring of inventories in e.g. tanks and silos spread all over the world
Operating systems
Windows 10 ® (Enterprise)
Windows 11 ® (Enterprise)
Windows Server 2016 (Standard)
Windows Server 2019 (Standard)
Windows Server 2022 (Standard)
Active Scripting enabled
JavaScript enabled
Allow cookies
Processor type
4 cores, 3 GHz or better
Main memory
8 GB (free memory)
Hard-disk capacity
50 GB for full installation, depending on database size
Monitor resolution, display
1280 x 800 (Desktop), application can also be used on mobile devices
1280 x 800 (Desktop), application can also be used on mobile devices
Interfaces
Business System via IMS Middleware
Web Browser
Business System via IMS Middleware
Web Browser
OPC DA Server
Elemica B2B Hub
Other
SupplyCare Enterprise runs by default in an Apache Tomcat-environment on an application server as service under Microsoft Windows. The operators and administrators operate the application via web browser from theirs desks.
Graphics: The minimum requirements do not take into account the requirements for the server operating system or other applications (e.g. antivirus software) installed on the server. The actual requirements and product functions can depend on the system configuration and the operating system. The requirements for the hardware will depend greatly on the desired number of users, failsafe performance etc..
SupplyCare Hosting runs securely in an Apache Tomcat-environment on an application Server in the "Cloud" hosted and maintained by Endress+Hauser. The operators and administrators operate the application via web browser from theirs desks.
Registered Trademarks
The following trademarks are either registered trademarks or trademarks of Microsoft Corporation in the United States and/ or other countries:
Microsoft®
Windows®
Windows Server®
The following trademarks are either registered trademarks or trademarks of Google LLC:
Google™
Google Chrome™
Google Maps™
The following trademarks are either registered trademarks or trademarks of Cisco Systems, Inc. and/ or its affiliates in the United States and certain other countries:
IOS®
Safari®, iPhone® and iPad® are trademarks of Apple® Inc., registered in the United States and other countries.
The following trademarks are either registered trademarks or trademarks of Microsoft Corporation in the United States and/or other countries:
Microsoft®
Windows®
Windows Server®
The following trademarks are either registered trademarks or trademarks of Google LLC:
Google™
Google Chrome™
Google Maps™
The following trademarks are either registered trademarks or trademarks of Cisco Systems, Inc. and/ or its affiliates in the United States and certain other countries:
IOS®
Safari®, iPhone® and iPad® are trademarks of Apple® Inc., registered in the United States and other countries.