De kan filtrere Deres søgning på sprog ved at vælge i listen 
Dokumentation (5)
Beskrivelse Version Sprog
Case Studies (CS)
1. Erfolgsstory Alvotech
Erfolgsstory zur Raman-Messung von Biosimilars in Downstream-Prozessen
03/25 Tysk
2. 拉曼光谱技术在生物仿制药下游工艺中的应用
成功案例 Alvotech 公司在超滤 / 渗滤过程中执行蛋白质纯化测试
10/24 Kinesisk
3. ラマン分光によるバイオシミラーのダウンストリームプロセス測定
- 限外ろ過/透析ろ過(UF/DF)におけるAlvotech社のタンパク質
精製プロセス監視

このケーススタディでは、Alvotech社がUF/DF中のダウンストリー
ムのタンパク質精製プロセスを監視するために、ラマンシステム(
RamanRxn2アナライザ、Rxn-10プローブ、ラマンフローアセンブリ)
をどのように活用したかを考察しています。
10/24 Japansk
4. Raman downstream process measurement of biosimilars -
Alvotech's monitoring of the protein purification process
during ultrafiltration / diafiltration (UF/DF)

This case study examines Alvotech's use of Raman systems
(Raman Rxn2 analyzer with Rxn-10 probe and Raman flow assembly)
to monitor the downstream protein purification process during UF/DF.
09/24 Tjekkisk
5. Raman downstream process measurement of biosimilars -
Alvotech's monitoring of the protein purification process
during ultrafiltration / diafiltration (UF/DF)

This case study examines Alvotech's use of Raman systems
(Raman Rxn2 analyzer with Rxn-10 probe and Raman flow assembly)
to monitor the downstream protein purification process during UF/DF.
06/24 Engelsk